Issue:
How to connect an HMIGTO to a Micrologix 1400 PLC?
Product Line:
Magelis HMIGTO
Resolution:
The cable combination to use is: Dsub9 [PLC side] <-- XBTZ9730 + XBTZG999 + D25 to D9 Converter (generic) --> Dsub9 [HMI Side]
You can also use XBTZ9730 + XBTZG919
How to connect an HMIGTO to a Micrologix 1400 PLC?
Product Line:
Magelis HMIGTO
Resolution:
The cable combination to use is: Dsub9 [PLC side] <-- XBTZ9730 + XBTZG999 + D25 to D9 Converter (generic) --> Dsub9 [HMI Side]
You can also use XBTZ9730 + XBTZG919
Released for: Schneider Electric Nigeria