Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to work with the individual objects inside a Grouped Object?
Issue:
Modfiying a grouped object is very tedious if we have to ungroup it first, make the changes to the individual objects and then regroup.

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, you don't need to ungroup Grouped Objects in order to modify them. To work with the individual objects of a grouped object, you can make use of the Graphics List tab of the Feedback Zone Window. In this Graphics List tab, you can expand each grouped object to show its sub-objects. Choose the exact object you wish you modify and change its settings as desired.