Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a Unity Pro / Control Expert .DTX file?

Issue:

What is a Unity Pro / Control Expert .DTX file?

Product Line:

Unity Pro, Control Expert, PLC

Resolution:

From the Control Expert menu:  PLC - Save/Restore data between a file and the PLC

Data Transfer allows you to store the value of the following data in a file that can be downloaded to or uploaded from a PLC.
%M
%MW
unlocated variables
function block instances

Restoring data from a .DTX file is allowed even if the application has been built and/or data has been modified since 'Save Data from PLC to  File' was performed.
(This is not possible if the data has been saved to a .DAT file.  For this reason, we recommend saving to a .DTX file).

In order to 'Save Data from PLC to File', the following must be true:
- PLC has a project loaded.
- PLC is in RUN or STOP mode.
- Unity Pro is running and connected to the PLC
- The project is built and is EQUAL to the PLC.

In order to 'Restore Data from File to PLC, point to the .DTX file that was previously saved.

NOTE:  I/O and Device DDT objects cannot be saved in DTX files.
SFC variables cannot be restored.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)