How can we help you today?

Do IU_ERIO work on X80 drop

Question:
An IU_ERIO function block updates Ethernet remote I/O drop input and output modules with an optimal response time. The Ethernet remote I/O drop inputs and outputs are updated during the MAST task.
In Unity help, the illustration example is only made in terms of Quantum Ethernet remote system(140CRA31200) .
Do this function block work on X80 drop(BMXCRA321x0)

Answer:
Yes.
After the verification test, this block is working in the Quantum X80 system.
By executing the block in MAST task, the output STATUS pin is properly indicating the drop status.