Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an Altivar drive be used to power up a panel or a device other than an AC motor?
Issue:
Altivar drive used to power up a panel or a device other than an AC motor.

Product Line:
All drives

Environment:
All

Cause:
Power conversion to power up a piece of panel equipment.

Resolution:
No. Altivar drives are designed to run AC squirrel cage inverter duty-rated motors only.
Please contact your local drives PAE (Product Application Engineer) for any  possible solutions.