Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can EcoStruxure Web Services (EWS) client send control commands back to Power Monitoring Expert (PME) Server?
Issue:
While connecting to PME via an EWS client, customers might have concerns over what actions the EWS client can perform on the PME software and the meters connected to the software.

Product Line:
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment:
EWS Client Configuration

Cause:
There might be concern over the EWS client connecting to the PME server and performing control actions such as resetting various values on a meter.

Resolution:
The only action a client can take is to request data and acknowledge alarms. In order to have external software send control commands through EWS to PME we would need an EWS client implementation in PME, which we do not have. We only have an EWS server in PME.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings