Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
I have a new Magelis BOX PC and the UPS/backup battery alarm is ON. I do not have the battery, how to I disable the alarm?
Issue:
I have a new Magelis BOX PC and the UPS/backup battery alarm is ON.  I do not have the battery, how to I disable the alarm?

Product Line:
Magelis BOX PC

Resolution:
Go to Control Panel > System Monitor > Properties > Battery.
Change the settings to disable the buzzer first, check apply.
Then disable the battery function to get rid of the dialog box, check apply.
(If it is not done in this order the buzzer may stay on).