Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we deliver oil distribution transformers in one piece without dismantling any part?
This is possible for up to 3,15MVA hermetically sealed corrugated wall distribution transformers. However, this will change for flat wall tank gas cushioned transformers with radiators. Depending on the design of the transformer, starting from 1,6MVA, the relevant transformers may have to be dismantled (radiators, cable boxes if there are any, terminal box, oil barrels, piping hardware, etc.) due to the dimensional constraints of the relevant containers. This will increase the delivery costs since you may have to switch to a high cost carrier equipment such as low bed truck for land delivery or flat rack container for overseas delivery. Please liaise with your relevant plant tendering consultant.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings