Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum protection level for TRIHAL cast resin dry type transformer?
The maximum protection level for Trihal cast resin dry type transformer is IP- 44.