Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the prerequisite Windows components required to install Vijeo Designer v6.2?
Issue:
What are the prerequisite Windows components required to install Vijeo Designer v6.2?

Product Line:
Vijeo Designer

Resolution:
Vijeo Designer v6.2 requires the following prerequisite software:
Windows Installer 4.5 for Windows XP SP2 and later (x86)
Microsoft Visual C++ 2005 SP1 Redistributable Package (x86)
Windows Installer 4.5 Update for Windows XP SP3 and later (x86)
Windows Installer 3.1 (x86)
Windows Imaging Component (x86)
Windows Installer 3.1 for Windows Server 2003 SP1 (x86)
Windows Imaging Component (x64)
Windows Installer 3.1 for Windows Server 2003 SP1 (IA64)
Windows Installer 3.1 for Windows Server 2003 SP1 (x64)
Windows Installer 3.1 for Windows XP (x64)
Microsoft .NET Framework 4.0 Full
Microsoft Visual C++ 2008 SP1 Redistributable Package (x86)