Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you power up the ATV312 with an external 24VDC supply?
Issue:
ATV312 powered up with external 24VDC supply

Product Line:
Altivar 312, ATV312

Environment:
All

Cause:
3-phase power not available. There may be a need to program the drive before shipping it to an end customer, for example.

Resolution:
No, the ATV312 drives cannot be powered up using an external 24VDC power supply.