Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the part numbers for the RJ45 Modbus cables for Schneider drives and soft starters?
VW3A8306R03 -  0.3 meter length cable / 1 foot
VW3A8306R10 - 1 meter length cable / 3 feet
VW3A8306R30 - 3 meter length cable / 9 feet

NOTE:  These cables will not work for connecting a remote mounted keypad for the drives/softstarts.
The best cables for remote keypad connections are:
VW3A1104R10 - 1 meter long / 3 feet
VW3A1104R30 - 3 meters long / 9 feet
VW3A1104R50 - 5 meters long / 15 feet
VW3A1104R100 - 10 meters long / 30 feet

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: