Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the max current for the +24v internal supply on the ATV61 drive?
Issue:
Max current for the +24v internal supply on the ATV61/71 drive.

Product Line:
All ATV61/71 drives

Environment:
+24v internal power supply on ATV61/71 drive

Resolution:
Max current for the internal +24v supply is 200mA.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings