Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ENM 8.3 Installation Manual
Issue
Customer would like to locate the ENM 8.3 installation manual.

Product Line
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0

Environment
ENM 8.3

Cause
Procedure for ENM installation

Resolution
See Attachment

*Note: As of PME 2020, an updated ENM configuration was introduced. The Integrated Event Notification Module includes a new notification engine that seamlessly integrates with PME for alarm-based notification.*

Schneider Electric Nigeria

Attachment(s)
ENM 8.3 Installation Guide.pdf [2.14 MB]