How can we help you today?

If a HMIG3U unit fails, can I pull the System SD Card from the failed unit and insert it into the replacement unit and will power-up?

Issue:
If a HMIG3U unit fails, can I pull the System SD Card from the failed unit and insert it into the replacement unit and will power-up?

Product Line:
HMIG3U

Resolution:
Yes, if a HMIG3U unit fails.  You can pull the System SD Card from the failed unit and insert it into the replacement unit with the same model number.  The unit will power-up and boot to the application.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre