{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Error thrown while activating Power Monitoring Expert license "Request includes activation IDs for a parent license and an update license that cannot be processed together in a single request"

Issue:
When attempting to activate a Power Monitoring Expert license using the Floating License Manager, there is an error thrown indicating "Request includes activation IDs for a parent license and an update license that cannot be processed together in a single request"

Product Line:
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0

Environment:
Power Monitoring Expert Software Configuration

Cause:
This is a screen capture of the error that will be seen:

License Request File denied

This is because the Activation IDs included in the license request contain an activation ID for the PME base license as well as for a Segment Edition (Buildings, Data Center, and HealthCare) Cross Grade license.

Resolution:
This is an example of two activation IDs that will be included in the Entitlement Certificate that can cause this error:

Activation ID: A-LN26-####-####
Description: PME-STD Base

Activation ID: A-4B8L-####-####
Description: DC Base Cross Grade

When trying to license a Segment Edition, we only require the Segment ID. In order to resolve this error, license the activation IDs again without including the PME-STD Base activation ID.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: