Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why the bluetooth interface TCSWAAC13FB does not restart after a power cut when is connected to the PLC TM221
As described in the Hardware Guide of SoMachine Basic, the PLC TM221xx RJ-45 connector with RS485 has some pins that MUST not be connected: Pins 1,2,3 and 6.
Please do not use 8 wires cables, use the cable reference XBTZ9980 (4 wires cable).