How can we help you today?

How to resolve the E5006 failure during Unity application upload.

Question:
Customer met with E5006 failure during Unity application upload. What's the root cause & how to solve it?


Answer:
The application is corrupted in the PLC   ( the conf tree is Invalid )

There are 2 ways to restore :

1. If the user has saved correctly the  application before ( it seems that it is not the case ) , rebuild all the application to FIX  then,  download  ( using Current Unity Version )

2. The customer  (or support ) can  use old Unity version    to upload  application. Then must  rebuild  all to fix the problem  (save  to  STA  ) or export  (to XEF) and finally use current version to re open  ( STA or XEF )