Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How does Vijeo Designer Runtime determine when to use Simulated SRAM?
Issue:
How does Vijeo Designer Runtime determine when to use Simulated SRAM?

Product Line:
Vijeo Designer (all versions)

Resolution:
Today in Vijeo Designer, there isn't any link between the data location settings and where the SRAM simulation file is actually stored. In fact, there is a series of checks that are done to determine the best place to store this internal file.
The algorithm is something like this:
if HMI has physical SRAM chip:
--> Start Runtime normally and use SRAM chip
If HMI has no physical SRAM chip:
check existence of Secondary Drive
--> If exists, store Simulated SRAM file on Secondary
--> else check existence of Optional.
--->If exists, store file on Optional
--->else error and refuse to start Runtime

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings