Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do you set up the ATV61/71 drive so that the set point for PID can be adjusted using the keypad?

Article available in these languages: Spanish

Issue:
Trying to set up the ATV61/71 drive so that the set point for PID can be adjusted using the keypad.

Product Line:
ALTIVAR 61, ALTIVAR 71

Environment:
All serial numbers

Resolution:
In the PID Regulator function, set parameter "Act. Internal PID ref" to NO.  Use "Ref 1 channel" set to HMI.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)