Issue
What does Error 1832 mean in Vijeo Designer v6.2?
Product Line
Vijeo Designer v6.2
Environment
HMI Configuration Software
Cause
The full message is:
Error 1832: [Target] [target name] Not enough space on target machine to download all application files. Check the Main, Secondary, and Optional drives.
This means the download has been interrupted because the destination drive for the Application on the target machine is full or unavailable.
Resolution
1) Download to a drive with more free memory on the target machine.
2) Erase or format the disk you want to download to and then download again.
The location of the User Application to be downloaded to is set from the Target > Options > Data Locations [...] button:
For non-Windows HMI:
Main Drive - Embedded Flash ROM memory
Secondary Drive - SD Card or CF Card (depending on the model of the HMI)
Optional Drive - USB Memory Stick
For Windows HMI (iPCs):
Main Drive - Depending on the model, this can be an SSD, HDD, or Embedded EEPROM which is C:\ and houses the Windows OS
Secondary Drive - Drive letter other than C:\ (can be a USB stick, external drive, another internal disk)
Optional Drive - Drive letter other than C:\ (can be a USB stick, external drive, another internal disk)
Released for:Schneider Electric Nigeria