Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to program the ATV71 drive to run from local control (keypad)?
Issue:
How to program ATV71 to run from local control?

Product Line:
Altivar 71, ATV71

Environment:
All

Cause:
N/A

Resolution:
Select the Drive menu.
Go to 1.6 Command, menu.
Set Ref 1 channel to HMI.
Set Profile to Not Separate.