Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I program a logic input for freewheel stop on an ATV12 drive?

Article available in these languages: Spanish

Issue:
Program a freewheel stop input on an ATV12 drive.

Product Line:
ATV12, Altivar 12

Environment:
All models

Cause:
N/A

Resolution:
The freewheel stop function is often used as a run permissive.
Freewheel stop (NST) can be assigned to a logic input by navigating to the CONF menu, then FUN menu, then STT- menu, and select parameter NST.  Assign it to the desired logic input by selecting either L1L, L2L, L3L, or L4L.   This function is active low and will cause the drive to enter freewheel stop mode and display NST on the screen when the logic input is low.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings