Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the operating system on the Harmony HMIGTO series?
Issue:
The user manual of the Hamrony HMIGTO does not indicate what operating system is pre-installed from the factory.

Product Line:
Harmony HMIGTO series (formerly known as Magelis)

Resolution:
The Harmony HMIGTO series of HMI's have the Operating System VxWorks V6.7 embedded inside.