Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an low torque alarm on the ATV61 or ATV71 drive?
Issue:
ATV61 and ATV71 low torque alarm causes.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Drive is triggering the low torque alarm

Resolution:
If there is a logic output assigned to (ttL) Low torque threshold I/O menu and the drives motor torque drops below the set or programmed threshold (50%) then the drive will trip or flash low torque threshold.

You would normally set this if you want to monitor if a belt breaks or if the motors torque drops below a set threshold.

Low torque thd setting.