Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to update M580 application from CPUv1.xx to v2.0?
In Unity v10's release notes:
(**) A M580 application with CPU V1.1x (developed with Unity Pro V8.0 or 8.1, or 10.0)  cannot be updated to CPU V2.0 : due to compatibility issues, the “Change CPU” option is not allowed. The proposed solution is to export/import variables and program into a new application.