Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you change the default display setting on an ATV12 drive?
Issue:
ATV212 default display adjustment

Product line:
ATV12, Altivar 12

Environment:
All

Cause:
n/a

Resolution:
The default display for the ATV12 will show Output Frequency.  To change this, enter into the Monitor menu (NOn).  Select the desired value you would like to see.  Push Enter a second time on that value and it will save your setting.

Some common options are:
rFr - Output Frequency
Frh - Reference Frequency
ULn - Line voltage
LCr - motor current

For further options, please consult the User Manual, document number BBV28581

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings