Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Latest firmware version for the energy server Com'X 510 (Version 6.8.7)
Issue
What is the latest firmware version for the Com'X 510?
Product Line
Com'X 510
EBX510

Environment
Firmware
Resolution
As of 05/07/2024, the latest version of firmware for the Com'X 510 is v6.8.7. This version is only required for Com'X 510 devices connected to the cloud. For non-cloud connected Com'X 510 devices, upgrading to firmware 6.8.4 provides the latest features and fixes. Both firmware versions can be downloaded from the links below:

Note: Depending on the existing Com'X 510 firmware version, it must be upgraded in stages to v2.1.17, then to v3.6.3, then to the latest version. The referenced firmware files are attached to this article below.
  • If the firmware version is older than v2.1.17, it must be upgraded to v2.1.17 first.
  • If the firmware version is newer than v.2.1.17, but older than v3.6.3, it must be upgraded to v3.6.3 first.

Refer to the following article for instructions to upgrade the firmware:

Schneider Electric Nigeria

Attachment(s)
ComX510_v2.1.17.zip [43.63 MB]
ComX510v3-6-3_Firmware_EBX510.zip [50.38 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings