Issue
BMXART0814 appears to be consuming two additional registers.
Product Line
BMXART0814
Environment
Unity, Control Expert
Resolution
If you configure a BMXART0814 and an analog module (e.g., BMXAMI0810) with no gap in the state ram assignment between the
two modules, the first two registers of the analog will appear not to work or overwritten.
The reason this occurs is because the BMXART0814 reserves two additional registers for the cold junction.
The workaround is to allocate a two register gap between the two modules.
BMXART0814 appears to be consuming two additional registers.
Product Line
BMXART0814
Environment
Unity, Control Expert
Resolution
If you configure a BMXART0814 and an analog module (e.g., BMXAMI0810) with no gap in the state ram assignment between the
two modules, the first two registers of the analog will appear not to work or overwritten.
The reason this occurs is because the BMXART0814 reserves two additional registers for the cold junction.
The workaround is to allocate a two register gap between the two modules.
Released for: Schneider Electric Nigeria