Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SoMachine 4.3 - how to connect to a controller without forcing a download

There are three files that are important to connect as equal or without forcing you to re-download a SoMachine 4.1 project. They are .bootinfo, .bootinfo_guids and .compileinfo.

1. These files are generated when you Login for the first time to the PLC and the boot application is created.

2. These files will change in the following situations:
- you make a change to the code and you execute Online / Create boot application or execute Multiple download / Always perform full download.
- you execute Build / Clean or Clean all and you execute Online / Create boot application or execute Multiple download / Always perform full download. This happens because Build / Clean or Clean all  deletes those three files

3. If you execute a File / Source download, it is important to do it after those three files were generated. If asked, select the option to include them in the source download files.

4. Alternatively you can create an archive by going to the SoMachine Central screen / Top-Left Green wheel / Save Project as... / Save Archive after those three files were generated. Opening the archive at a later time will ensure that those files are kept together and that a connection without download is possible.

5. For a particular project you can automate the source download. The option is available under the Logic Builder / Project / Project Settings / Source Download / Timing

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)