How can we help you today?

How to reconfigure the application of 140ERT85420 from S908 RIO to QEIO.

There are some ERT configured in Quantum S908 RIO station. After user upgraded the system from S908 to QEIO, the ERT EFB STATUS is 16#5000 that means Wrong Slot. The health bit of ERT module is "1"(OK).
Check the EFB configuration in the application, Found the issue is the number of Drop configuration error. In S908 system the first Remote IO drop number is 2, but in EIO system the frist default value of drop is 1; so customer is easy to have this error if they copied their application program from a old S908 system.

Change the number of the drop from 2 to 1, the ERT work correctly.
The picture is in attachment

Schneider Electric Nigeria

Attachment(s)
ERT config.jpg [126.53 KB]