How can we help you today?

How to connect the TSXNTP100 to 140ERT85420 for clock synchronization

Some user can't find the diagram of the connection guidle for TSXNTP100 and 140ERT85420. Some can find the data sheet of NTP100 but it is failure with the clock synchronization.
please refer to this notes for them. which had been verificated in lab.
I get the pin of RJ45 for RS485 of TSXNTP100 from R&D. you should connect the PIN5(RJ45) to PIN38(ERT), PIN4(RJ45) to PIN40(ERT).
There is a mistake of the doc, you should exchange the PIN4 and PIN5

Schneider Electric Nigeria

Attachment(s)
RJ45 of NTP100.jpg [15.32 KB]