How can we help you today?

To configure a Profibus Remote Master with a M580 PLC range, a channel number must be define. The help of UnityPro doesn't deliver the channel number for a M580 PLC range. => Which channel to select?

If the PRM (Profibus Remote Master) is configured as a DIO in a M580 PLC, the channel number "03" must be configured in the PRM management Function Bloc.

Schneider Electric Nigeria