Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to understand the speed of NOE and NOC
some user found the communication speed of NOE and NOC is different. E.g. download same application to PLC by Quantum NOE is faster than NOC. NOC needs 2 times of NOE.
Why, the reasons as following
(1) NOC78100 has router which is implemented in f/w => because of this feature (weather enabled or disabled) we take performance hit

(2) Bandwidth limitations => ports have bandwidth limitation to protect the system, which also causes download speed to slow.
You must remember that the NOC and the NOE are not the same type of module.  The NOC has both MB TCP/IP as well as EIP and therefore has many more feature built into the code base.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings