Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
HTTP SSL Functionality in Power Monitoring Expert

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

Issue
How to setup HTTP SSL and communicate over port 443 with the Power Monitoring Expert software modules and disable HTTP (port 80). The web browser on the client computer issues a message to the users indicating that the SSL certificate has not been issued by a trusted certificate authority.

Web Certificate Error

Product Line
StruxureWare Power Monitoring Expert

Environment
Power Monitoring Expert 7.2

Power Monitoring Expert 8

Power Monitoring Expert 9.x

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Cause
The Secure Socket Layer (SSL) protocol allows you to establish an encrypted link between your Web server and a browser to protect login credentials and data from interception by a 3rd party on the network. To create an SSL connection, your Web server requires an SSL Certificate.

Resolution
By default, HTTP SSL (HTTPS) functions are enabled out-of-the-box with Power Monitoring Expert software. All of the components within PME including Application Modules, Web Reporter and WebReach can be accessed through HTTPS over port 443.

In order enforce the use of HTTPS and disable access over HTTP with Power Monitoring Expert, an HTTP filter or firewall must be setup on the server or network level. To maintain proper functionality of PME, do not disable HTTP support within IIS (Internet Information Services). It is recommended that HTTP access to the server be blocked but rather not disable HTTP support.

The Web Applications component (consisting of Dashboards, Diagrams, Alarms, Tables, and Reports) can be accessed via SSL by specifying "https" instead of "http" in a Web browser on a client computer. For example:

https://domain_name/Web

where domain_name is the fully-qualified name of the server hosting Power Monitoring Expert and Web is the default root directory, which can be changed during installation. Alternatively, you can use the IP address of the server.

**Note: Web browsers on client computers may issue a message to users indicating that the SSL certificate has not been issued by a trusted certificate authority. To remove this warning and improve the security of your system by creating an SSL connection, it is recommended that you acquire and install a certificate from a certificate authority. You can install the certificate by following the instructions here.

Configure PME for hosting PME over HTTPS/HTTP via the FAQ: https://www.se.com/us/en/faqs/FA309041/.