Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use CSH 120 and CSH 200 to all Sepam series 10 models?
CSH120 and CSH200 modules cannot be used with all Sepam series 10 models because they can only be used with Sepam 10XX3X versions. These are Sepam 10 versions with very sensitive earth fault protection.

AEDL3