Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to activate an event task with the BMX EHC 0200/0800 modules?
An Event task can only be activated in the BMX EHC 0200 or BMX EHC 0800 when the module is in the main local rack or in an extended local rack
and the I/O data type is Topological.

The event task can be activated in the configuration screen of the module:

Enable Event
Choose the event task number to be activated.