There are two possibilities for this problem.
1. The head of the firmware was damaged, so it couldn’t recognize the hardware ID of the PLC and the firmware couldn’t be loaded.
2. The hardware was damaged, maybe the MCU or the memory.
For these two possibilities, customer can't do anything but only replace the PLC.
Released for: Schneider Electric Nigeria