Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When I put base station in the metal enclosure, how much will transmission distance be shortened? (Max 50m?)
It will depends on the shape, dimension, type of metal, thickness and so on of the enclosure.