Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use the same switchboard case across the ION8xxx meter series?
Issue
The compatibility of switchboard cases across the ION8nnn meter series.

Product Line
PowerLogic ION8300, ION8400, ION8500, ION8600, ION8650 meters

Environment
Advanced Revenue Metering

Cause
The user would like to use the pre-existing switchboard case when replacing the meter.

Resolution
Provided that if the replacement meter and the switchboard enclosure share the same form factor, theen the two are interchangeable.