Background:
Customer is using TSXCBY380KT for a project which requires large amounts of data transmission
The datesheet of TSXCBY380KT has no announcement of transmission capacity.
Question:
Could TSXCBY380KT transmit data over 1Mbyte per second?
Answer:
Yes, it could transmit data over 1Mbyte per second from cable SPEC
Customer is using TSXCBY380KT for a project which requires large amounts of data transmission
The datesheet of TSXCBY380KT has no announcement of transmission capacity.
Question:
Could TSXCBY380KT transmit data over 1Mbyte per second?
Answer:
Yes, it could transmit data over 1Mbyte per second from cable SPEC
Released for: Schneider Electric Nigeria