Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
New Release of PM3200 driver for PME 8.0 and Register List

Issue
A client has upgraded the PM3200 meter to firmware 1.2.003 and thus not supported in PME 8.0.

Product Line
Power Monitoring Expert 8.0 with PM3200 meter

Environment
Driver update in PME 8.0

Cause
This update resolves the following issues:

- Alarms were not being downloaded after alarm log roll-over.
- Jitter correction for onboard logs (+/- 5 secs)

Resolution
The SE package includes the PM3200 driver for the "PME 8.0.exe" executable file. The release notes document and the mapping details/register list are attached below

To install the driver, follow the steps below:

1. Run the 'PM3200_Series_SE_8.0.15355.01_Setup.exe' file that you can find in the Related tab.
2. Select the preferred language and click 'Next' to proceed with installation.
3. Follow the on-screen procedure to verify the system, prepare for upgrade by performing backups and configure the system.
4. Once the installation is complete, click Close to exit. The update driver should now appear under 'Device Types' within Management Console.

Comments:

This issue was resolved by SE in PME versions released after 8.0

Schneider Electric Nigeria

Attachment(s)
PM3200_Series_SE_8.0.15355.01_Setup.exe [4.34 MB]
PM3200_Series_SE_8.0.15355.01_Mapping.xlsx [73.98 KB]
PM3200_Series_SE_Driver_Release_Notes_PME 8.0.pdf [3.06 MB]