Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to "Move" One Variable to Another in SCADAPack Workbench (ST, FBD and LD)
Some PLC programming applications have a "move" block to perform the task of assigning one variable to another. In SCADApack Workbench (CAM3 & CAM5) there are multiple programming language options as it is an IEC 61131-1 environment. Each of these languages have their unique way of performing a "move" command

In the following examples it is assumed you have declared local variables for each POU (Program Organization Unit)

1

Function Block Diagram (FBD)

2

Structured Text (ST)

3

Ladder Diagram (LD)

4