How can we help you today?

What are the Modbus functions that can be done with Sepam 10 A version?

Issue

A user wants to know which Modbus communication functions are available in the Sepam Series 10 A protection relay.

Product

  • Sepam Series 10 A

Environment

  • Sepam Series 10 A with Modbus communication
  • Remote monitoring and control applications
  • Industrial power distribution systems

Cause

Users may require clarification regarding the Modbus communication capabilities of the Sepam Series 10 A, particularly when integrating the relay into a supervisory or monitoring system.

Resolution

The Sepam Series 10 A supports a limited set of Modbus communication functions. The available functions include:

  • Remote controlling of the device.
  • Reading time-tagged events.
  • Reading measurements.
  • Time and date setting.
  • Time synchronization.

The Sepam Series 10 A Modbus communication capability is restricted to these monitoring, control, and time management functions.