Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a conformal coating option for the HMIGTU series?
Yes, the Magelis HMIGTU series are available with conformal coating. Part numbers shown below:

HMIG3UFC Premium Box
HMIG5UFC Open Box

HMIDT351FC 7" Screen
HMIDT542FC 10.4" Screen
HMIDT551FC 10" Screen
HMIDT642FC 12.1" Screen
HMIDT651FC 12" Screen
HMIDT732FC 15" Screen