Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
'Could not start DTM' error gets returned when updating the catalog upon opening Unity.
Issue
'Could not start' DTM error gets returned when updating the 'DTM Catalog Content' upon opening Unity.

Product Line
EcoStruxure Control Expert (formerly known as Unity Pro)

Environment
Windows 7 Professional, Unity Pro v10

Resolution
If you install a new DTM and then open Unity, it returns the message asking if you want to update the DTM Catalog. Duringthe update, it must start the DTM.  If it fails to start, the message '....Could not start DTM' will get returned in a DTM Catalog content window.  (This scenario also applies if you install a new version of Unity.)



This could occur if you have a 32 bit Windows operating system and a large amount of software or DTM installed on the PC. When the DTM catalog is updated, it opens the DTM's that are provided with Unity and any other third party DTM's that are also installed on the PC.  Some third party DTM's also launch their own DTM software when the DTM is started. If the PC does not have enough free memory, the DTM will not start.

To resolve the issue:
-Close any processes running in the background that are not needed..
-Add more memory to the PC.
-Uninstall any third party DTM and software that is not needed.
-Update to 64 bit operating system.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings