The braking unit module part number VW3A7005 is listed in our catalogs and is the correct part number in most of the world.
However, in the USA this part is not available. Instead, we use part number VW3A11701.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
Released for: Schneider Electric Nigeria