Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What terminals are a braking resistor connected to on the ATV61/71 drives?
Issue:
Braking resistor terminals connected to on the ATV61/71 drives.

Product Line:
Altivar 61, Altivar 71

Environment:
All ATV61's and ATV71's up to Frame size 12

Cause:
N/A

Resolution:
A braking resistor should be connected to terminals PA+ and PB on all VFDs up to frame size 12. Frame sizes 13 and higher require a brake transistor.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings