Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of Modbus/TCP slave device words for TM258 / LMC058 and TM241 / TM251 controllers in SoMachine or Machine Expert?

Starting with SoMachine 4.1 SP2 a new firmware version: 4.0.2.xx was delivered. In this new version the maximum size of words increased for Modbus TCP slave device: %IW 120 words - %QW 120 words (previously 40 input / 40 output words).

Notes:
- The above information is correct also for Machine Expert 1.x and 2.x
-  EcoStruxure Machine Expert supports M258 and LMC058 controllers starting with version 1.2.5. Previous version of EcoStruxure Machine Expert did not support them.
- EcoStruxure Machine Expert v2.0 does support M258 or LMC058 controllers anymore.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings