Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the bandwidth requirement of Unity and Quantum
See screen shot of screen to configure (in this case I choosed to allow 12 x 1024 requests ==> it means 12 requests of a maximum length of 1024 bytes for each, by/per MAST cycle).
This parameter concern all requests sent by UnityPro to PLC, for animation, but also download, upload...etc

This parameter will impact the bandwidth between Unity and Quantum, you can calculate the min bandwidth requirement as per this parameter.

Schneider Electric Nigeria

Attachment(s)
Untitled.jpg [238.52 KB]